Skip to main content

Redefining Automation with Physical AI

Moving from digital intelligence to embodied autonomy in the physical world

Image Source: Ventura/stock.adobe.com; generated with AI

By Abhishek Jadhav for Mouser Electronics

Published March 26, 2026

Artificial intelligence (AI) has undergone significant advancements over the past two decades. Early AI systems were designed for data-driven tasks such as image recognition, language processing, and predictive analytics. Today, AI is moving from the digital realm to being embedded into physical machines.

The convergence of AI with robotics and automation represents the next evolution in industrial operational technology: physical AI. This concept comprises autonomous robotics systems with AI capabilities that can perceive their environment, make intelligent decisions, and act in the physical world.

The development of physical AI is driven by the recent breakthroughs in machine learning (ML) algorithms, sensor technologies, and computing hardware. All of these elements enable a new generation of more intelligent and adaptable machines that can substantially improve efficiency and flexibility across various industries.

This article examines the shift of AI from the digital realm to the physical world, the various factors driving this change, and where the technology may ultimately lead.

Breakthroughs in AI

The resurgence of modern AI can be traced back to the 2010s with the introduction of deep learning. In 2012, deep neural networks achieved impressive results in visual object recognition, demonstrating that machines could learn complex patterns from large datasets. This catalyzed a wave of innovation in AI, from convolutional neural networks (CNNs) to reinforcement learning.

By the late 2010s and early 2020s, AI models had grown exponentially in scale and capability. A key breakthrough came with language models and vision transformers, which can generate human-like texts and recognize images with high accuracy. However, all of these capabilities were confined to the digital domain for analyzing data and automating virtual tasks.

In industrial automation, AI has been applied in two key application areas: analytics and predictive maintenance. ML models can sift through vast volumes of data (e.g., from sensors on production lines, quality inspection cameras, and supply chain systems) to detect patterns or anomalies that humans might miss.

AI offers a more intelligent approach for predictive maintenance by monitoring equipment condition in real time through vibration sensors, temperature readings, and oil analysis, and by applying ML to predict failures before they occur. Switching from reactive maintenance to AI-based predictive strategies can reduce unplanned downtime by 30 to 50 percent and cut maintenance costs by up to 40 percent.[1]

Despite the efficiency that traditional AI use cases bring, the true potential of AI lies in bringing intelligence to the physical world. Advances in computer vision, robotics hardware, and edge computing are making this possible. This transition marks the beginning of the physical AI era.

What Is Physical AI?

Physical AI is an AI system embodied in physical machines and devices that enables them to autonomously sense, reason, and act in the real world. For instance, a warehouse robot using physical AI might perceive boxes through its camera, decide which box to pick up next, and then physically move and place the box using its robotic arm.

Physical AI refers to AI that has a physical presence enabling it to interact with its surroundings, as opposed to AI that exists only as software. Physical AI systems integrate a range of technologies, including advanced perception systems (such as computer vision, lidar, and auditory sensors), reasoning and decision algorithms to interpret sensor data and plan actions, and actuation mechanisms to execute those actions.

To better understand physical AI, it is important to differentiate it from traditional robotics. Traditional industrial robots are largely rule-based and pre-programmed systems that repeatedly execute a set of instructions with high precision. They could not adjust if conditions changed. Due to a robot’s rigidity by design, an operator would have to reprogram it to perform new tasks, which would incur additional downtime.

Another key difference is real-time perception. Traditional robots, even those equipped with closed-loop control systems for precise feedback, often lack adaptive perception and context-aware decision-making capabilities. Physical AI devices are equipped with modern perception systems, including high-resolution cameras, depth sensors, and tactile sensors, which allow them to “see” and “feel” what they are doing.

In essence, physical AI brings flexibility and adaptability to robotics that were previously absent. That said, traditional rule-based robots remain useful for highly structured tasks. Instead of simply replacing legacy robots, physical AI robots will augment and expand the capabilities of automation. But as tasks become more complex and variable, the advantages of physical AI make it the foundation of next-generation automation systems.

Factors Driving the Adoption of Physical AI

Several converging factors, both on the demand side (industry needs) and on the supply side (technology enablers), are driving companies to adopt physical AI solutions.

Labor Shortages and Rising Costs

Many industries, especially manufacturing and logistics, are facing workforce challenges. In the wake of global supply chain disruptions and reshoring efforts, Western manufacturers are facing skilled labor shortages,[2] underscoring the need to intensify their use of automation to remain competitive.

Physical AI provides a way to fill the widening skills gap by automating tasks that are difficult to staff. Intelligent robots can operate around the clock without fatigue, helping industries control labor costs and meet throughput targets. In short, economic trends are making the business case for advanced automation stronger than ever.

Need for Flexibility and Resilience

Traditional AI automation is rigid. It struggles with high product variety or sudden changes. Markets today are volatile with shorter product lifecycles and rapidly changing consumer preferences. As such, manufacturers need flexible automation that can adapt to various products and small batch sizes without necessitating extensive retooling each time.

Physical AI enables this flexibility by allowing robots to be re-tasked or to handle variability through learning. These robots can also provide resilience by automating critical tasks and reducing reliance on human availability.

Simulation and Digital Twin Technology

A critical enabler for the adoption of physical AI is the ability to train and test machines in simulation before deploying them in the real world. High-fidelity simulators, such as NVIDIA Isaac Sim, can create digital twins of robots and their operating environments. These digital twins offer two primary benefits: They enable the safe and scalable use of techniques like reinforcement learning and significantly reduce development and deployment time for new robotic solutions.

As simulation tools continue to improve with realistic physics and synthetic data generation, they act as a force multiplier for physical AI. Even small and medium-sized enterprises can leverage simulation-driven development to adopt intelligent robots without massive in-house research and development.

Physical AI Use Cases

Autonomous vehicles are one of the most visible manifestations of physical AI. These self-driving vehicles are essentially robots on wheels, perceiving the road using cameras, light detection and ranging (lidar), and radar. They use AI to interpret the scene, make driving decisions, and control the steering and braking accordingly.

Physical AI also has the potential to transform the most complex industry: healthcare. Nvidia recently collaborated with GE HealthCare to develop autonomous diagnostic imaging with physical AI.[3] The collaboration aims to develop an X-ray and ultrasound system that can position the patient, scan, and check image quality with minimal human intervention.

Another interesting use case comes from space exploration, where extreme conditions prevent humans from performing some operations. Instead, physical AI can step in to perform dangerous, complex tasks. It is no longer just an assistive tool but an important partner in humanity’s push to the stars. Together with humans, these technologies are opening doors to a new world.

Conclusion

Physical AI stands at the forefront of the fifth industrial revolution, combining digital intelligence of AI with the tangible capabilities of machines. By embracing physical AI, we move toward a world where machines are not just automated but truly autonomous.

The journey has only begun; as physical AI technologies continue to evolve, they will undoubtedly redefine what automation looks like in the coming decades.

 

Sources

[1]https://www.mckinsey.com/capabilities/operations/our-insights/manufacturing-analytics-unleashes-productivity-and-profitability
[2]https://www.ascm.org/ascm-insights/scm-now-impact/manufacturing-labor-shortage-threatens-u.s.-nearshoring-efforts
[3]https://nvidianews.nvidia.com/news/nvidia-and-ge-healthcare-collaborate-to-advance-the-development-of-autonomous-diagnostic-imaging-with-physical-ai

About the Author

Abhishek Jadhav received his M.S. in Electrical and Computer Engineering and began his career as a technical writer. He has over five years of experience working as a freelance technical writer, with key interests in power electronics and embedded systems. His work has appeared in EE Times, embedded.com, and Power Electronics News, among others.

Profile Photo of Abhishek Jadhav